Mouser Press Room
Mouser Facebook Mouser Twitter Mouser RSS Feed Mouser YouTube Channel Mouser Google+ Mouser LinkedIn Mouser Subscription Center Mouser Blog
Mouser Press Room
New Product Announcement

 

Harwin's Kona High-Reliability Power Connectors, Now Available at Mouser, Ensure Maximum Power in Harsh Environments

May 6, 2021 - Mouser Electronics, Inc., the authorized global distributor with the newest semiconductors and electronic components, is now stocking the new Kona high-reliability power connectors from Harwin. Capable of delivering 60 A of continuous current per contact, the highly durable connectors can support battery charging applications without needing to divide the current across multiple contacts.

The Harwin Kona connectors, now available from Mouser, feature a six-finger beryllium copper contact design with full gold plating in an 8.5 mm pitch. The connectors are individually shrouded on both male and female versions, preventing accidental touching and physical damage. Designed for use in harsh environments, the Kona power connectors rely on a rugged cable-to-board design to maintain electrical continuity during heavy vibration and shock. Featuring stainless steel thumb screws on the female connector housing, the power connectors can be easily repaired without any tools required.

The Kona connectors also use an innovative mate-before-lock mechanism which ensures contacts are fully mated before engaging fixings. The robust connectors offer a durability of 250 mating cycles, a wide operating temperature range of -65°C to 150°C, and a 5 kV maximum voltage rating.

The Kona power connectors are available in a single row of two-, three-, or four-contacts, and are ideal for a range of uses in extreme conditions, including power control systems, robotic drives, electric vehicle battery monitoring and management, satellites, and UAVs.

To learn more, visit https://www.mouser.com/new/harwin/harwin-kona/.


As a global authorized distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed customers' designs, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Center, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser
Mouser Electronics, a Berkshire Hathaway company, is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, Mouser.com, is available in multiple languages and currencies and features more than 5 million products from over 1,100 manufacturer brands. Mouser offers 27 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 630,000 customers in 223 countries/territories from its 1 million-square-foot, state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About Harwin
Harwin is a manufacturer of High Reliability Interconnects suitable for harsh environments and are able to withstand extreme vibration, shock and temperature. Datamate, Gecko and M300 product lines have a proven history in Military, Aerospace and other safety critical markets. Other board level solutions include EMC Shielding products which increase reliability, flexibility and cost savings through the process of automated placement. Industry standard connectors and PCB hardware are also available from Harwin for commercial applications.

Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.



Further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
(817) 804-3833
Kevin.Hess@mouser.com
For press inquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com
Back to Press Room